Dear Technical support team,
1. I would like to know what is the units of the ADC's sampling frequency listed in the sysfs entries,
By default I see the sampling frequency as 58098 , Is that the 58098 is 58.098KHz or what is the units of 58098???
Kindly let me know what is units of the the below values as well
cat sampling_frequency_available
206250 58098 29676 15000 7541
2.
- Is it possible to verify that whether the ADC is operating in one shot or continuous mode using linux sysfs entries, if so how can we switch between continous and one shot mode using sysfs entries?
- The below is the different sysfs attributes for ADC, can we switch between continuous and one shot mode using in_conversion_mode?
root@imx6ull14x14evk:/sys/bus/iio/devices/iio:device0# ls
buffer in_voltage3_raw sampling_frequency_available
dev in_voltage_sampling_frequency scan_elements
in_conversion_mode in_voltage_scale subsystem
in_voltage0_raw name trigger
in_voltage1_raw of_node uevent
in_voltage2_raw power
As am stuck in finding the units from past many days, kindly do the needful as early as possible