Reference Manual IMX7DRM.pdf [ MIPI DSI Host Controller (MIPI_DSI) 13.4.3.9.4 Buffer ]
What is the unit of buffer described in this?
For example, for a 480 [H] x 800 [V] monitor
1. HSYNC period 1LINE = 480
2. VSYNC period 1 image = 384000 [480x800]
----------------------------------------------------------------------------------------------------------------------
13.4.3.9.4 Buffer
In MIPI DSI standard specification, DSI Master sends image stream in burst mode. The
image stream transmits in high-speed and bit-clock frequency. This mode allows the
device to stay in stop state longer to reduce power consumption. For this mode, MIPI DSI
Master has a line buffer to store one complete line and send it faster at the next line time.