What is the right way to run weston

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the right way to run weston

9,417 Views
alexeykuzmin
Contributor II

I just build wayland image for IMX6QP evaluation board, put weston.ini file and try to run weston.

But it black screen and following error. What to do?

root@imx6qpsabresd:~# weston
Date: 2018-09-05 UTC
[17:01:56.899] weston 1.11.0
               http://wayland.freedesktop.org
               Bug reports to: https://bugs.freedesktop.org/enter_bug.cgi?product=Wayland&component=weston&version=1.11.0
               Build: 1.10.93-2-g2d825ed configure.ac: bump to version 1.11.0 for the official release (2016-05-31 17:10:40 -0700)
[17:01:56.900] OS: Linux, 4.9.11-1.0.0+gc27010d, #10 SMP PREEMPT Fri Sep 7 16:46:00 MSK 2018, armv7l
[17:01:56.901] Using config file '/home/root/.config/weston.ini'
[17:01:56.902] Output repaint window is 7 ms maximum.
[17:01:56.902] Loading module '/usr/lib/weston/fbdev-backend.so'
[17:01:56.933] initializing fbdev backend
[17:01:56.934] logind: failed to get session seat
[17:01:56.934] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[17:01:56.935] <stdin> not a vt
[17:01:56.935] if running weston from ssh, use --tty to specify a tty
[17:01:56.935] fatal: fbdev backend should be run using weston-launch binary or as root
[17:01:56.935] fatal: failed to create compositor backend
root@imx6qpsabresd:~#

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

6,794 Views
joanxie
NXP TechSupport
NXP TechSupport

for weston, I suggest that you can refer to the document first

Weston Introduction for I.MX 

https://community.nxp.com/docs/DOC-95380 

0 Kudos
Reply