What is the purpose of unit test?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the purpose of unit test?

3,324件の閲覧回数
kangmw086
Contributor III

hi

i used imx6q.

 

What is the purpose of unit test?

 

PATH = /unint_test/V4L2

mxc_v4l2_capture.out

mxc_v4l2_output.out

mxc_v4l2_overlay.out

mxc_v4l2_still.out

What is the purpose of each?

 

thank you.

 

 

ラベル(5)
0 件の賞賛
返信
6 返答(返信)

3,318件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

 

unit tests are simple tests for various i.MX modules, can be used for example for

testing custom hardware (camera, lcd, e.t.c.). Sources and description of usage can be found on:

https://source.codeaurora.org/external/imx/imx-test/tree/?h=lf-5.10.y_2.0.0

 

Best regards
igor

0 件の賞賛
返信

3,309件の閲覧回数
kangmw086
Contributor III

Thank you for your reply.

But the answer I want to get is...

mxc_v4l2_capture.out, mxc_v4l2_output.out, mxc_v4l2_overlay.out, mxc_v4l2_still.out

 

I want to know what 4 execute file each do.

For example, 

mxc_v4l2_capture.out -> camera capture?

mxc_v4l2_output.out -> camera preview?

 

thank you.

0 件の賞賛
返信

3,303件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can look in documentation (README, ../doc) in

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test?h=lf-5.10.y_2.0.0

 

Best regards
igor

0 件の賞賛
返信

3,292件の閲覧回数
kangmw086
Contributor III

Could you provide me with another source code to test the camera?

There was no answer to my question, so please check it.

 

https://community.nxp.com/t5/i-MX-Processors/I-MX-qtapplication-source-code-question/td-p/1303460

 

regards!

0 件の賞賛
返信

3,280件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>Could you provide me with another source code to test the camera?

 

also one can try baremetal sdk test (1.1.0_iMX6_Platform_SDK.zip) from link

https://community.nxp.com/t5/i-MX-Processors/SMP-Enable-in-IMX6/m-p/542111

 

Best regards
igor

0 件の賞賛
返信

3,267件の閲覧回数
kangmw086
Contributor III

Thank you for giving me the SDK test code.

Can you provide me with the application code made of QT?

I've run the qcamera example, but the UI doesn't appear.

I would like to download the IMX-QTAPPLICATION source code included in YOCTO(x11). 

--> imxcamera application.

This software is available in bin files only. Can you provide me with the source code?

 

thank you.

0 件の賞賛
返信