hi
i used imx6q.
What is the purpose of unit test?
PATH = /unint_test/V4L2
mxc_v4l2_capture.out
mxc_v4l2_output.out
mxc_v4l2_overlay.out
mxc_v4l2_still.out
What is the purpose of each?
thank you.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi
unit tests are simple tests for various i.MX modules, can be used for example for
testing custom hardware (camera, lcd, e.t.c.). Sources and description of usage can be found on:
https://source.codeaurora.org/external/imx/imx-test/tree/?h=lf-5.10.y_2.0.0
Best regards
igor
Thank you for your reply.
But the answer I want to get is...
mxc_v4l2_capture.out, mxc_v4l2_output.out, mxc_v4l2_overlay.out, mxc_v4l2_still.out
I want to know what 4 execute file each do.
For example,
mxc_v4l2_capture.out -> camera capture?
mxc_v4l2_output.out -> camera preview?
thank you.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		one can look in documentation (README, ../doc) in
https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test?h=lf-5.10.y_2.0.0
Best regards
igor
Could you provide me with another source code to test the camera?
There was no answer to my question, so please check it.
https://community.nxp.com/t5/i-MX-Processors/I-MX-qtapplication-source-code-question/td-p/1303460
regards!
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		>Could you provide me with another source code to test the camera?
also one can try baremetal sdk test (1.1.0_iMX6_Platform_SDK.zip) from link
https://community.nxp.com/t5/i-MX-Processors/SMP-Enable-in-IMX6/m-p/542111
Best regards
igor
Thank you for giving me the SDK test code.
Can you provide me with the application code made of QT?
I've run the qcamera example, but the UI doesn't appear.
I would like to download the IMX-QTAPPLICATION source code included in YOCTO(x11).
--> imxcamera application.
This software is available in bin files only. Can you provide me with the source code?
thank you.