What is the purpose of TSENSOR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the purpose of TSENSOR?

Jump to solution
1,245 Views
adevries
Contributor V

Hello,

On the 8M Mini processor, there are two pins I'm curious about, TSENSOR_TEST_OUT and TSENSOR_RES_EXT. What is the purpose of these pins? Do they need to be connected to anything? The datasheet, reference manual, and hardware design guide don't really talk about them.

Thanks

Labels (1)
Tags (2)
1 Solution
1,097 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello adevries,

These pins are factory used only so TSENSOR_TEST_OUT leave floating and TSENSOR_RES_EXT connect over 100k to the GND.

Regards

 

View solution in original post

2 Replies
1,097 Views
eagan
Contributor I

Can you please add this to the documentation? I was unable to find it in any of the available i.MX 8M Mini docs.

1,098 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello adevries,

These pins are factory used only so TSENSOR_TEST_OUT leave floating and TSENSOR_RES_EXT connect over 100k to the GND.

Regards