What is the purpose of R667 in the Sabre schematics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the purpose of R667 in the Sabre schematics

744件の閲覧回数
dougschwanke
Contributor IV

I understand that this is a DNP part, but I am wondering why the part was even on the schematic.  We have a lot of customers who replicate this design and are placing pads on the board.

When would someone pull this pin down? 

My current assumption is that it is related to designs where the user uses 4 data lines and DAT3/CD share the same pin, such as micro SD cards.

ラベル(1)
0 件の賞賛
2 返答(返信)

641件の閲覧回数
dougschwanke
Contributor IV

Based on http://www.nxp.com/documents/application_note/AN10911.pdf [^] page 17, the Micro SD card has built in pullup resistor on CD/D3 pin (10Kohm - 90Kohm).

NXP recommended an external pull-down resistor should be 270Kohm or higher.  Since the Sabre schematic (SPF-27392_C3) lists 10K, I have ask if this has ever been tested in the lab.

0 件の賞賛

641件の閲覧回数
dougschwanke
Contributor IV

Populating this resistor did not fix our problem of Linux detecting the 4-bit interface. 

0 件の賞賛