What is the part name/part number of FPC (Interface cable -30PIN ) used in SABRE board to connect LVDS1 and Display panel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the part name/part number of FPC (Interface cable -30PIN ) used in SABRE board to connect LVDS1 and Display panel

1,770 Views
sreeharshap
Contributor II

Hello there,

What is the part name/part number of FPC (Interface cable -30PIN ) used in SABRE board  to connect LVDS1 and Display panel?.

FYI please find the attachment image reference of the cable on IMG_5859.JPG                                                                                                                                                                                                                                                                                     SABRE board.

Regards

Pole

0 Kudos
Reply
3 Replies

1,659 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pole,

The connector is DF19G-30P-1H(56), Manufacturer: HIROSE. In the hardware you can refer to our SPF-27392_C3.pdf design file. And the link for the connector is as follows:

DF19G-30P-1H(56) Hirose Connector | Mouser
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,659 Views
sreeharshap
Contributor II

Hi Dan、

Thanks so much for your kind response.

Wonderful day!!

Pole

0 Kudos
Reply

1,659 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pole,

It's my pleasure:smileyhappy:. If you have new questions you can create new threads in our community, here could you help close this one.

Have a nice day

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply