What is the most up-to-date reference for understanding the device tree binary and how it is built?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the most up-to-date reference for understanding the device tree binary and how it is built?

ソリューションへジャンプ
2,718件の閲覧回数
EdSutter
Senior Contributor II

I'm running with SABRESDB in preparation for my custom hardware.

My custom hardware core is similar to SABRESDB; but I still wanna make sure I know how to build/modify the .dtb file.

I'm currently reading through the kernel's Documentation/devicetree/usage-mode.txt and also http://devicetree.org/Device_Tree_Usage,

are these documentation sources the correct place to be reading up on the FDT stuff used with iMX6/SabreSDB or is there

additional/other places to get better acquainted with this?

Thanks in advance,

Ed

EDIT---

Perhaps a more fundamental question is: will I need to modify the .dts file for custom iMX6 hardware or is this file something that describes the SOC/CPU and its IO independent of the circuitry around the SOC?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,841件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ed,

A .dts file describes a particular board. You can start with imx6qdl-sabresd.dtsi, for example and adapt it to your own board.

You can see how other mx6  boards are supported in device tree: ls -al arch/arm/boot/dts/imx6*

Regards,

Fabio Estevam

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,842件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ed,

A .dts file describes a particular board. You can start with imx6qdl-sabresd.dtsi, for example and adapt it to your own board.

You can see how other mx6  boards are supported in device tree: ls -al arch/arm/boot/dts/imx6*

Regards,

Fabio Estevam

0 件の賞賛
返信
1,841件の閲覧回数
EdSutter
Senior Contributor II

Fabio,

Ok, I've been looking at this since I posted the question.  I see the .dts file is processed by 'dtc' (device-tree-compiler i assume?)

to generate the .dtb file.  Does this binary translate into runtime initialization in the kernel somewhere?

One other question...

I noticed an option in kernel menuconfig: "Use appended device tree blob to zImage (EXPERIMENTAL)".

Does this do what it implies; thus eliminating the need to download the separate .dtb file and using the 3-argument bootm command?

Thanks much,

Ed

0 件の賞賛
返信
1,841件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Hi Ed,

Yes, when you run "make imx6q-sabresd.dtb' , the dts file is converted to the dtb binary.

Just replied in more details about the appended device tree in another thread.

Regards,

Fabio Estevam

0 件の賞賛
返信