What is the most up-to-date reference for understanding the device tree binary and how it is built?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the most up-to-date reference for understanding the device tree binary and how it is built?

Jump to solution
2,895 Views
EdSutter
Senior Contributor II

I'm running with SABRESDB in preparation for my custom hardware.

My custom hardware core is similar to SABRESDB; but I still wanna make sure I know how to build/modify the .dtb file.

I'm currently reading through the kernel's Documentation/devicetree/usage-mode.txt and also http://devicetree.org/Device_Tree_Usage,

are these documentation sources the correct place to be reading up on the FDT stuff used with iMX6/SabreSDB or is there

additional/other places to get better acquainted with this?

Thanks in advance,

Ed

EDIT---

Perhaps a more fundamental question is: will I need to modify the .dts file for custom iMX6 hardware or is this file something that describes the SOC/CPU and its IO independent of the circuitry around the SOC?

Labels (1)
0 Kudos
Reply
1 Solution
2,018 Views
fabio_estevam
NXP Employee
NXP Employee

Ed,

A .dts file describes a particular board. You can start with imx6qdl-sabresd.dtsi, for example and adapt it to your own board.

You can see how other mx6  boards are supported in device tree: ls -al arch/arm/boot/dts/imx6*

Regards,

Fabio Estevam

View solution in original post

0 Kudos
Reply
3 Replies
2,019 Views
fabio_estevam
NXP Employee
NXP Employee

Ed,

A .dts file describes a particular board. You can start with imx6qdl-sabresd.dtsi, for example and adapt it to your own board.

You can see how other mx6  boards are supported in device tree: ls -al arch/arm/boot/dts/imx6*

Regards,

Fabio Estevam

0 Kudos
Reply
2,018 Views
EdSutter
Senior Contributor II

Fabio,

Ok, I've been looking at this since I posted the question.  I see the .dts file is processed by 'dtc' (device-tree-compiler i assume?)

to generate the .dtb file.  Does this binary translate into runtime initialization in the kernel somewhere?

One other question...

I noticed an option in kernel menuconfig: "Use appended device tree blob to zImage (EXPERIMENTAL)".

Does this do what it implies; thus eliminating the need to download the separate .dtb file and using the 3-argument bootm command?

Thanks much,

Ed

0 Kudos
Reply
2,018 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Ed,

Yes, when you run "make imx6q-sabresd.dtb' , the dts file is converted to the dtb binary.

Just replied in more details about the appended device tree in another thread.

Regards,

Fabio Estevam

0 Kudos
Reply