What is the most recent (newest) version of Ubuntu that correctly supports the ltib tools, etc...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the most recent (newest) version of Ubuntu that correctly supports the ltib tools, etc...

1,647 Views
blsousan
Contributor III

All,

    What is the most recent (newest) version of Ubuntu that correctly supports the ltib tools, etc... for development on the iMX28 EVK?  I've seen references to 9.X  and to 10.4, but was wondering if there are newer versions of Ubuntu that correctly supports all hte iMX28 EVK tools?

Thanks,

Bill

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,582 Views
andrew_questps
Contributor III

I'm running a VM of 12.04 and got ltib compiling correctly (for imx25 though), although there are some changes that need to be applied to the ltib configuration before it will work. I just followed a few of the guides floating around the net and on here as to what patches needed to be applied to get it going.

0 Kudos
Reply