What is the maximum input voltage for VLDO34, in MC32PF3000A2EP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum input voltage for VLDO34, in MC32PF3000A2EP?

914 次查看
logeshs
Contributor II

In reference to What is the maximum input voltage for VLDO34, in MC32PF3000A2EP  

Currently we have connected as per Warp reference design. In Warp design, you have connected PMIC_PWR to VLDO34IN. Also, PMIC_PWR is ORed with VBAT. In this case PMIC_PWR will get >3.6V at full charge right? Will this damage the PMIC pin? Should we follow the datasheet or the reference design? Please refer the Warp schematic.

Thank you

标签 (1)
0 项奖励
回复
1 回复

790 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Logesh

it is necessary to follow the datasheet. Please note that sometimes

designs are developed when datasheets are not fully validated using some

preliminary data.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复