What is the mass for the i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the mass for the i.MX7D

Jump to solution
1,060 Views
geoffreyzeiss
Contributor IV

Hi,

What is the mass in grams for the i.MX7D processor in the 12mm square package? I cannot find it mentioned in the datasheet.

Thanks,
Geoff Zeiss

Labels (1)
1 Solution
974 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Geoff,

The mass is indicated on the Material Declaration document of each part number. For example, for MCIMX7D7DVK10SD (which is a 12x12mm package) is available here.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

View solution in original post

1 Reply
975 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Geoff,

The mass is indicated on the Material Declaration document of each part number. For example, for MCIMX7D7DVK10SD (which is a 12x12mm package) is available here.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------