What is the i.MX7 ADC inputs' absolute max voltage rating?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the i.MX7 ADC inputs' absolute max voltage rating?

1,029 次查看
alixmaldonado
NXP Employee
NXP Employee

Absolute max should not to be confused with max operating voltage (listed as 1.89V in data sheet). 

Bottom line: will the ADC input get damaged if it is exposed to 3.3V?

i.mx7‌

标记 (1)
0 项奖励
回复
1 回复

921 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Alix,

The ADC inputs should be between high and low analog reference voltages. In case of the i.MX7, it is from 0V to max 1.9V (Table 93 of i.MX7 Datasheet, shown below).

imx7 adc.png

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复