The imxs6dlrm manual (04/2015) is not clear on this function. On page 2932 it says:
"The DP_GWSEL bit defines if the BG is the pixel coming from the full plane or the partial plane."
On page 3269 it says:
"GWSEL - Graphic Window Select"
"Select graphic window to be on partial plane or full plane."
Please clarify.
Thanks. So "graphic window" means BG (background plane)?
DP_GWSEL bit determins which plane used for graphic window, when DP_GWSEL=0, dev/fb0(full plane) is used for BG, this is default in BSP, when DP_GWSEL=1, dev/fb1(partial plane) is used for BG.