I'm comparing information obtained from the iMX7 Reference Manual (Rev. 0.1, 08/2016) and the iMX7D SABRE development board schematics (rev D). They show different definitions for the BOOT_CFG pin 6:4, when booting from an SD/eMMC device.
The Reference Manual (Table 6-41) says that BOOT_CFG[6:4] define the Bus Width, and to use a value of 0 - SD/eSD/SDXC, and value of 1 for MMC/eMMC.
Page 18 of the schematics says that for eMMC, BOOT_CFG[6:4] define the bus width (000 - 1 bit, 001 - 4 bit, etc...) and that for SD, BOOT_CFG[6:4] defines the bus width (000 - 1 bit, 001 - 4 bit, all other values reserved).
Which is correct, the reference manual or the SABRE eval board schematics ?
已解决! 转到解答。
Hello,
Please use information of the iMX7D SABRE development board schematic.
The Reference Manual will be changed in next release.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
Hello,
Please use information of the iMX7D SABRE development board schematic.
The Reference Manual will be changed in next release.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!