What is the difference between MCIMX93-EVK board and the MCIMX93-EVKCM board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between MCIMX93-EVK board and the MCIMX93-EVKCM board?

524 Views
Z2025121
Contributor II

By ordering a board from distributors, I see both MCIMX93-EVK and MCIMX93-EVKCM are available. What are difference between these two boards?

Are the power consumption tests (AN13917) applicable only for one of the board?

Thanks

0 Kudos
Reply
2 Replies

511 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The MCIMX93EVKCM is obsolete and no longer manufacturer you need to get the MCIMX93EVK since it comes with the new silicon version A1.

Regards

0 Kudos
Reply

487 Views
Z2025121
Contributor II
Thanks.
0 Kudos
Reply