What is the difference between MCIMX27MOP4A and MCIMX27MJP4A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between MCIMX27MOP4A and MCIMX27MJP4A

1,044 Views
Kai1900
Contributor I

Hello,

I saw in datasheet, MCIMX27OP4A and MCIMX27JP4A have same temperature and package. May I know the difference between them? 

Shall I directly replacement them one by another?

39ADAEBC-23E8-4E75-B352-3DC3F21F7FAC.png

Tags (1)
0 Kudos
Reply
1 Reply

1,036 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

MO = 19x19mm, 0.80mm,
MAPBGA 473,
-40°C to +85°C

The difference between the O and the J in the part numbers is a historical die attach difference that's now been unified to the same die attach. The two sets of part numbers were retained because it was logistically easier for the various customers using each. Yes, you can replacement them each other as the packages are also the same. Hope this can do help for you.

 

0 Kudos
Reply