What is the OTG PWR Enable default value for iMX7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the OTG PWR Enable default value for iMX7?

Jump to solution
1,543 Views
davidsabalesky
Contributor I

What is the default OTG Power Enable signal for iMX7?

Can this value be changed in Uboot?

Can this value be change at the Uboot prompt?

My USB OTG1 port VBUS is not becoming active with ID set low, host mode.

We have a custom carrier pcb where the USB switches are active high.

Any help is greatly appreciated.

Labels (2)
0 Kudos
Reply
1 Solution
1,400 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi David,
For additional details regarding USB recommendations, you could take a look at “Hardware Development Guide for the i.MX7D and i.MX7S Applications Processors”.
For complementary details, you could take a look to the following Community threads:

usb-otg1 without id pin on 3.14.28 

USB OTG support in IMX6Q 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you

-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,401 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi David,
For additional details regarding USB recommendations, you could take a look at “Hardware Development Guide for the i.MX7D and i.MX7S Applications Processors”.
For complementary details, you could take a look to the following Community threads:

usb-otg1 without id pin on 3.14.28 

USB OTG support in IMX6Q 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you

-------------------------------------------------------------------------------

0 Kudos
Reply