What is the Cactus player for in the i.MX6 Freescale Android BSP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the Cactus player for in the i.MX6 Freescale Android BSP?

Jump to solution
4,474 Views
chetkaufman
NXP Employee
NXP Employee

We are working on a project to support a new customer wanting to develop a media player using Android and the i.MX6Q.   They are seeing several media players in the BSP including a Freescale developed Media Player called Cactus.  There does not appear to be any documentation on Cactus.  Why is Cactus player in the Freescale Android BSP?

Labels (3)
1 Solution
3,390 Views
JayTu
NXP Employee
NXP Employee

Cactus player is used to demo our multimedia extended features:

  • Trick mode playback (fast forward, fast rewind)
  • Multiple audio track selection at run time
  • Subtitle and selection

View solution in original post

3 Replies
3,390 Views
YixingKong
Senior Contributor IV

Chester

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply
3,390 Views
chetkaufman
NXP Employee
NXP Employee

Yes, thanks the question is answered now.

Thanks,

Chet Kaufman

www.freescale.com

425-478-9285

0 Kudos
Reply
3,391 Views
JayTu
NXP Employee
NXP Employee

Cactus player is used to demo our multimedia extended features:

  • Trick mode playback (fast forward, fast rewind)
  • Multiple audio track selection at run time
  • Subtitle and selection