Hi community,
Our partner have a question about i.MX6SDL IPU CSI.
Please see page 2818 in IMX6SDLRM Rev.2, it shows the following sentence.
Unpacking and companding capabilities are provided for up to two streams (either through same or different interfaces), while the other ones are treated as generic data.
Then, we don't understand what is "unpacking and companding capabilities".
Would you kindly let us know what is it?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hi Satoshi
"unpacking and companding capabilities" mean usage
Data Packing Unit described in Figure 38-15 CSI Block Diagram
and Table 38-16 Packing Unit, that is input data can be unpacked -
converted to a IPU common internal 8/16-bit format. Unpacked data
with more than 8 bits per sample may be optionally companded,
generating 8-bit samples. Description is given in sect.38.4.3.5 Companding.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
"unpacking and companding capabilities" mean usage
Data Packing Unit described in Figure 38-15 CSI Block Diagram
and Table 38-16 Packing Unit, that is input data can be unpacked -
converted to a IPU common internal 8/16-bit format. Unpacked data
with more than 8 bits per sample may be optionally companded,
generating 8-bit samples. Description is given in sect.38.4.3.5 Companding.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------