What is i.MX6Q ECSPI min frequency?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is i.MX6Q ECSPI min frequency?

848 Views
shkolnyykonstan
Contributor III

I have an SPI device that can work maximum at 400Hz.

Is it possible to configure ECSPI to this frequency?

Labels (1)
0 Kudos
Reply
1 Reply

777 Views
igorpadykov
NXP Employee
NXP Employee

Hi Konstantin

from i.MX6 side there is no limitation, just to set

appropriate source ccm  pll value.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply