What is i.MX6 IPU DI display clock polarity?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is i.MX6 IPU DI display clock polarity?

ソリューションへジャンプ
1,503件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a questions about i.MX6 IPU DI display clock polarity.

Please see chapter 38.5.193 in IMX6SDLRM Rev.1.

There is di0_polarity_disp_clk field, and description says as below.

=====

DI0 Output Clock's polarity

This bits define the polarity of the DI0's clock.

1 The output clock is active high

0 The output clock is active low

=====

But I did not understand what are "active high" & "active low".

What is changed by changing this polarity?

(e.g. active high = latch on rising edge, active low = latch on falling edge)

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
1,226件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, it would be better to say the output clock is inverted or not.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,227件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, it would be better to say the output clock is inverted or not.

0 件の賞賛
返信