We were exploring role switch for imx8qm-Android9-Auto.
I came to know that role switch can be possible by changing right role (host | gadget) in
/sys/bus/platform/devices/ci_hdrc.0/role
已解决! 转到解答。
Hi Amit
there are two USB controllers:
- One is USB2 compatible and the IP comes from ChipIdea (the same USB IP used on mx5/mx6/mx7)
- One is USB3 compatible and the IP comes from Cadence.
The Cadence USB controller is described like this in arch/arm64/boot/dts/freescale/imx8-ss-conn.dtsi:
usbotg3: usb3@5b110000 {
compatible = "Cadence,usb3";
....
The Chipidea USB controller is described like this in arch/arm64/boot/dts/freescale/imx8-ss-conn.dtsi:
usbotg1: usb@5b0d0000 {
compatible = "fsl,imx8qm-usb", "fsl,imx7ulp-usb",
"fsl,imx27-usb";
....
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Amit
there are two USB controllers:
- One is USB2 compatible and the IP comes from ChipIdea (the same USB IP used on mx5/mx6/mx7)
- One is USB3 compatible and the IP comes from Cadence.
The Cadence USB controller is described like this in arch/arm64/boot/dts/freescale/imx8-ss-conn.dtsi:
usbotg3: usb3@5b110000 {
compatible = "Cadence,usb3";
....
The Chipidea USB controller is described like this in arch/arm64/boot/dts/freescale/imx8-ss-conn.dtsi:
usbotg1: usb@5b0d0000 {
compatible = "fsl,imx8qm-usb", "fsl,imx7ulp-usb",
"fsl,imx27-usb";
....
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------