What is Kobs-ng?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,738件の閲覧回数
eunseokjung
Contributor II

Hi all,

I'm studying about u boot and this applications.

But i couldn't understand of this part. Especially , Kobs-ng and U-boot.

Kobs-ng includes FCB, DBBT, and UBoot image. Is this right? If it is right, how to use Kobs-ng?

I already downloaded latest version from Index of /buildsources/k/kobs-ng/kobs-ng-3.0.35-4.0.0

But i don't know how to use this. It is not execution file.

Please introduce document or site for learning about this.

Thank you.

ラベル(1)
0 件の賞賛
1 解決策
2,750件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eunseok

available commands can be found in main.c its sources,

usage is given in attached Linux Manual p.22.

Execution file wiil be available after bulding sources or

using Demo images:

Board Support Packages (5)

i.MX28 Linux Binary Demo Files (REV L2.6.35_1.1.0)

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
2,751件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eunseok

available commands can be found in main.c its sources,

usage is given in attached Linux Manual p.22.

Execution file wiil be available after bulding sources or

using Demo images:

Board Support Packages (5)

i.MX28 Linux Binary Demo Files (REV L2.6.35_1.1.0)

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛