What is Kobs-ng?

cancel
Showing results for 
Search instead for 
Did you mean: 

What is Kobs-ng?

Jump to solution
4,881 Views
eunseokjung
Contributor II

Hi all,

I'm studying about u boot and this applications.

But i couldn't understand of this part. Especially , Kobs-ng and U-boot.

Kobs-ng includes FCB, DBBT, and UBoot image. Is this right? If it is right, how to use Kobs-ng?

I already downloaded latest version from Index of /buildsources/k/kobs-ng/kobs-ng-3.0.35-4.0.0

But i don't know how to use this. It is not execution file.

Please introduce document or site for learning about this.

Thank you.

Labels (1)
0 Kudos
1 Solution
1,893 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eunseok

available commands can be found in main.c its sources,

usage is given in attached Linux Manual p.22.

Execution file wiil be available after bulding sources or

using Demo images:

Board Support Packages (5)

i.MX28 Linux Binary Demo Files (REV L2.6.35_1.1.0)

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
1,894 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eunseok

available commands can be found in main.c its sources,

usage is given in attached Linux Manual p.22.

Execution file wiil be available after bulding sources or

using Demo images:

Board Support Packages (5)

i.MX28 Linux Binary Demo Files (REV L2.6.35_1.1.0)

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos