What i.MX6DQ eFuses are burned by freescale?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What i.MX6DQ eFuses are burned by freescale?

Jump to solution
1,957 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6DQ eFuse.

We want to know whant eFuse is burned by freescale, and what eFuse should be burned by user.

Especially, we want to know about the eFuse values correspond to the following OCOTP registers.

OCOTP_ANA1

OCOTP_MAC0

OCOTP_MAC1

OCOTP_GP1

OCOTP_GP2

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,514 Views
gusarambula
NXP TechSupport
NXP TechSupport

You are correct, I apologize.

Fuses like the MAC address are up to the customer to program.

Other fuses are set at factory and those include OCOTP_ANA1 which has the temperature calibration information, you may find more details on Table 62-1 of the i.MX6DQ Reference Manual (link below).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

View solution in original post

0 Kudos
Reply
3 Replies
1,514 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Satoshi Shimoda,

Freescale’s processors ship with the eFuses intact unless it’s otherwise asked by the customer. The regular parts do not come with any eFuse programming; it is the customer’s responsibility to program these fuses.

I hope this information helps!

0 Kudos
Reply
1,514 Views
satoshishimoda
Senior Contributor I

Hi gusarambula,

I believe Freescale burns some eFuses when shipping.

For example, device  unique ID (0x410, 0x420), speed grading (0x440), temperature grade (0x480), etc...

I think Freescale should prohibit programming to these eFuses by user.

According to you reply, I guess OCOTP_MACx (0x620) and OCOTP_GPx (0x660, 0x670) are not programmed.

But I did not understand whether OCOTP_ANA1 is programmed and whether what is this because this is not described in Table 5-10 in IMX6DQRM (Rev.2).

So would you confirm what eFuse is programmed again?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,515 Views
gusarambula
NXP TechSupport
NXP TechSupport

You are correct, I apologize.

Fuses like the MAC address are up to the customer to program.

Other fuses are set at factory and those include OCOTP_ANA1 which has the temperature calibration information, you may find more details on Table 62-1 of the i.MX6DQ Reference Manual (link below).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

0 Kudos
Reply