What gstreamer1.0 element can be used with imxvideoconvert_g2d0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What gstreamer1.0 element can be used with imxvideoconvert_g2d0?

Jump to solution
1,326 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about gstremaer1.0 in i.MX6 Linux BSP.

I want to use imxvideoconvert_g2d gstremer1.0 element to resizing.

Then, I tried some elements with imxvideoconvert_g2d (e.g. imxv4l2src, ximagesrc) on L3.10.53_1.1.0-ga BSP, but it was failed with error such as the following message.

WARNING: erroneous pipeline: could not link imxv4l2src0 to imxvideoconvert_g2d0

Then, would you let me know what element is able to be used with imxvideoconvert_g2d0?

Best Regards,

Satoshi Shimoda1.

Tags (2)
0 Kudos
1 Solution
1,027 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

please refer to attached Linux Guide sect.7.5.4 Video Conversion

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
1,028 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

please refer to attached Linux Guide sect.7.5.4 Video Conversion

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,027 Views
satoshishimoda
Senior Contributor I

Hi Igor,

Yes, according to the document, I can understand videotestsrc elements can be used for source of imxvideoconvert_g2d.

Is that all?

Or can I use other element also for imxvideoconvert_g2d?

Actually, I want to use imxvideoconvert_g2d resizing of camera input.

But videotestsrc is not camera input I think.

Best Regards,

Satoshi Shimoda

0 Kudos
1,027 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes this all

Best regards

igor

1,027 Views
satoshishimoda
Senior Contributor I

Hi Igor,

OK, I understood.

Thank you for your support

Best Regards,

Satoshi Shimoda

0 Kudos