What does set i.MX6 HDMI display refresh rate?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What does set i.MX6 HDMI display refresh rate?

跳至解决方案
1,297 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6 HDMI.

You know HDMI display refresh rate are several.

(e.g. 60.00, 59.94, 50.00, 23,98 Hz, etc...)

Then, what register determin the refresh rate?

HDMI module does not control and IPU DI controls it by VSYNC?

Best Regards,

Satoshi Shimoda

标记 (1)
0 项奖励
回复
1 解答
930 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes IPU controls it by VSYNC, providing data to HDMI,

one can look at example in IMX6DQRM Figure 33-4 and appnote below

shows how refresh is defined in LInux:

AN3974 Different Display Configurations on i.MX35 Linux PDK

sect.3.3.1.2 Panel Configuration, refresh rate

HDMI.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
931 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes IPU controls it by VSYNC, providing data to HDMI,

one can look at example in IMX6DQRM Figure 33-4 and appnote below

shows how refresh is defined in LInux:

AN3974 Different Display Configurations on i.MX35 Linux PDK

sect.3.3.1.2 Panel Configuration, refresh rate

HDMI.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复