What does 0x80000000 exactly do in IOMUX CFG ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What does 0x80000000 exactly do in IOMUX CFG ?

2,655件の閲覧回数
glitch911
Contributor I

Hi all,

I've been reading with interest this post : understanding iomuxing imx6QD  but can't find the answer ;(

Can you point me to the source of this 0x80000000 value in IOMUX configuration?

More precisely I'd like to know if it's only the PAD_CTL that is unchanged or the MUX_CTL setting as well?

For example MX6QDL_PAD_EIM_D22__GPIO3_IO22 is supposed to set the EIM_D22 PAD as GPIO (ALT5) (#define in imx6q-pinfunc.h) but after changing u-boot to use USB OTG it seems that PAD_EIM_D22 is now configured as USB_OTG_PWR (ALT4) and MX6QDL_PAD_EIM_D22__GPIO3_IO22 0x80000000 seems to do nothing about that after leaving u-boot as I still read 4 when typing devregs 0x020e00a8 (MUX_CTL). For now I need to type "devregs 0x020e00a8 0x5" to get my USB power-supply started. It works but I'd like to understand better why ^^

Any help will be appreciated.

タグ(2)
2 返答(返信)

2,205件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

if you check the code drivers/pinctrl/freescale/pinctrl-imx.c, 0x80000000 will igore to configure the IOMUX and keep the value. And If  0x40000000 to set the SION. 


/* The bits in CONFIG cell defined in binding doc*/
#define IMX_NO_PAD_CTL 0x80000000 /* no pin config need */
#define IMX_PAD_SION 0x40000000  /* set SION */

more explaination.

If you want to add the SION, the original dts like this:

MX6UL_PAD_CSI_DATA01__GPIO4_IO22         0x17059

you need to modify and become

MX6UL_PAD_CSI_DATA01__GPIO4_IO22         0x40017059(0x40000000 |0x17059)

If you want to keep it. Just make  it 0x80000000 is enough.

2,205件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi glitch911

this is linux software convention, not hardware.

Please check linux documentation fsl,imx-pinctrl.txt

linux-imx.git - i.MX Linux Kernel 

Bits used for CONFIG:
NO_PAD_CTL(1 << 31): indicate this pin does not need config.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------