What camera application can we use for Windows 10 IoT Enterprise / iMX8M platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What camera application can we use for Windows 10 IoT Enterprise / iMX8M platform

7,585件の閲覧回数
hiron
Contributor II

I am now evaluating Windows 10 IoT W1.1.0, 6/2022 BSP release and successfully bring up the Windows 10 IoT GUI using 8MPLUSLPD4-EVK board.

When I connect USB UVC WebCam (Logitech C270n) to USB port, this camera silently recognized and appear in the Device Manager tree display.

But there appears no camera ready application exist in Windows 10 IoT Microsoft distribution. What camera application do you use for the development (in BSP camera team) ?

---

Below is my UWP application screen shot to take still picture, asking one application to handle camera data.  This UWP app works fine on both x64 notebook and ARM64 notebook though...

UWPDemo_IMX8PLUS2.png

 

 

 

 

タグ(2)
0 件の賞賛
返信
3 返答(返信)

7,530件の閲覧回数
hiron
Contributor II

Thanks for the replay. 


I just noticed that some pre-installed Windows (store) apps that are included in regular desktop Windows 10, such as "Windows Camera" and "App Installer", are missing in the "LTSC" release.

I am also surprised that , when the "Windows Camera App" is installed, the "CameraCaptureUI" C# class works!.

We have not yet checked, but the GAC version of Windows 10 IoT comes with several store apps pre-installed and should work just like regular Windows 10.

---

App Installer

https://www.microsoft.com/store/ProductId/9NBLGGH4NNS1  

Windows Camera App

https://www.microsoft.com/store/productId/9WZDNCRFJBBG 

 

 

0 件の賞賛
返信

7,573件の閲覧回数
hiron
Contributor II

From my further investigation, I checked preinstalled "Windows (store) app" in IMX8M Windows 10 IoT core, by using administrator account of PowerShell, explained below link.

https://docs.microsoft.com/en-us/windows/application-management/provisioned-apps-windows-client-os#u... 

I first tested in my Windows PC and found:

- Microsoft.DesktopAppInstaller Microsoft.DesktopAppInstaller_2022.728.1939.0_neutral_~_8wekyb3d8...

- Microsoft.WindowsStore Microsoft.WindowsStore_22207.1401.1.0_neutral_~_8wekyb3d8bbwe

but there is no such apps included in IMX8M Windows result (below).

PowerShell2.png

The only package "Microsoft.MicrosoftEdge.Stable" may be installed by Windows Update.

---

I believe some of the Windows (Store) app should be preinstalled in OOBE phase. But current BSP install script appears no apps to place, so that some of the user's UWP apps can't always duplicate the standard Desktop Windows experience.

0 件の賞賛
返信

7,548件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello hiron,

The win10IOT is the initial engineering release for i.MX6, i.MX7 and i.MX8M platforms you might found a lot of troubleshooting on it. in any case you may want to know more about it, please send a request to Microsoft.

 

Regards

0 件の賞賛
返信