What builds are available for the gpu-viv-bin-imx6q package?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What builds are available for the gpu-viv-bin-imx6q package?

1,977 次查看
jonathanolson
Contributor II

The Yocto distribution fetches a binary blob from http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/ which contains all the support for OpenGL and OpenCL in the Vivante GPU.  Unfortunately, these libraries don't work with the kernel GPU driver in later kernels and are build against eglibc.

Are there any builds for kernels later than 3.10?  Are there any builds which support uClibc?  Does Freescale have any plans to open-source the GPU code with the kernel and X11 to make it possible to update these components without compatibility issues with these binary-only components?

0 项奖励
回复
1 回复

1,451 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jonathan

one can look at Graphics recipes p.4 attached document

L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation

Regarding "open-source the GPU code",  note this is third party IP

(Vivante).

Best regards

igor

0 项奖励
回复