What are the i.MX28 LRADC Accuracy specifications?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What are the i.MX28 LRADC Accuracy specifications?

1,487 次查看
jschoen
Contributor III

Are there any specifications or characterization of the accuracy (DNL, INL, offset error, gain error, etc) for the i.MX28 LRADC?

标签 (1)
0 项奖励
回复
3 回复数

1,278 次查看
jackgrozev
Contributor I

Hi Igor,

The document you quote above states that the main reason for the relatively low accuracy of the LRADC (1.3%) is the bandgap reference and it can be calibrated using fuses. However I have read in another post that this calibration mechanism is actually not available. Is that true?

Also, I can't find any other specification about the LRADC such as linearity, acuracy performance (inluding accuracy and linearity) over temperature etc... Are these available? Where could I find them?

Thank you!

Kind regards:

jack.

0 项奖励
回复

1,278 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jschoen

accuracy is given in MCIMX28RM sect.38.1 LRADC Overview

MX28 LRADC.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,278 次查看
jschoen
Contributor III

Thanks Igor.

I was looking in the data sheet.  Didn't think to look in the RM for those specs.

Joel

0 项奖励
回复