What are the Voice Recognition options available in iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the Voice Recognition options available in iMX6

736 Views
keshavakumarb
Contributor I

Hello,

I want to know the voice detection/recognition support in imx6 via external microphone. How can I achieve this??

Thank you in advance.

Tags (3)
0 Kudos
Reply
1 Reply

567 Views
art
NXP Employee
NXP Employee

There are no any voice recognition acceleration capabilities on the hardware level in the i.MX6 series processors. All this is software dependent. For example, if you run Android, you can use its voice recognition/control capabilities etc.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply