What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EVK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EVK?

954 次查看
Iyshwarya
Contributor I

What are all the Linux-kernel versions which are compatible (so that I should not get any checkvinff error) with the Android 11.0.0_2.2.0 using i.MX8MQ EVK? And replacing the separately built kernel Image alone of the supported version to the Android source code helps me to upgrade the kernel?

0 项奖励
回复
1 回复

936 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the release note, android 11.0.0_2.2.0 uses Linux 5.10.35 kernel

0 项奖励
回复