Hi Bryan
yes, pin (W7; NVCC_1P2V) may be tied to the voltage you use for DDR
or use the same voltage value from other power source.
I did not fully understand question:
"what is the 1.2V power pin used for in the SoloLite".
Table 73 "13 x 13 mm Functional Contact Assignments"
SoloLite Datasheet (REV3) gives power domains for all pads.
Yes, NVCC_1P2V is used for the HSIC interface, others - not.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------