What Kinetis M4 would you use knowing the source had to migrate to i.MX6 SoloX?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What Kinetis M4 would you use knowing the source had to migrate to i.MX6 SoloX?

跳至解决方案
1,736 次查看
benhouston
Contributor III

We are currently evaluating and developing on the Kinetis K64.  Eventually, due to 5 year road map considerations, we would like to migrate the K64 binary over to an i.MX6 SoloX so that we can maintain the network with a Linux OS.  The real time functionality would stay intact and port over easily to the M4 core on the SoloX.

Is this even possible with the K64's or any of the Kinetis ARM M4's?  If so, which aligns best with the SoloX's M4?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,412 次查看
b36401
NXP Employee
NXP Employee

No. They are not binary compatible.

At least they have different memory maps.

You will need to compile the binaries again during the migration.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,412 次查看
benhouston
Contributor III

Thanks for the info.  This answers the main question.

0 项奖励
回复
1,412 次查看
lucianomoretti
Contributor IV

As Victor said, you'll have to recompile.  As long as you use an OS that runs on the M4 on both the Kinetis and the M4 SoloX core, plus stick to standard C and don't hardcode addresses porting should be a pretty easy: You'd have to change the BSP but none of your app code.

0 项奖励
回复
1,413 次查看
b36401
NXP Employee
NXP Employee

No. They are not binary compatible.

At least they have different memory maps.

You will need to compile the binaries again during the migration.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复