Weston problem on parallel lcd display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Weston problem on parallel lcd display

跳至解决方案
2,125 次查看
davideballestre
Contributor I

Hi,
we are running BSP 5.15.71_2.2.0 on a custom board with a parallel lcd display and imx6dl microprocessor. We are facing a problem with weston surface g2d-renderer. only vertical stripes are visible (see attached image).
It seems a pixel format problem but framebuffer is working well and weston logs are ok.
Without "use-g2d=1" weston fails to start with "failed to create egl surface" (see attached log).
Can you help me?

Thanks

Davide

标签 (1)
0 项奖励
回复
1 解答
2,088 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @davideballestre,

I hope you are doing well
 
My apology for the delayed response.
Please try to set the bpp value for the Weston to <16> from the device tree.
 
Thanks & Regards,
Dhruvit Vasavada

在原帖中查看解决方案

2 回复数
2,089 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @davideballestre,

I hope you are doing well
 
My apology for the delayed response.
Please try to set the bpp value for the Weston to <16> from the device tree.
 
Thanks & Regards,
Dhruvit Vasavada
2,069 次查看
davideballestre
Contributor I

hi!
everything well here! with your solution weston works great now (see attached image).

thank you very much for your help.

regards
davide

 

 

0 项奖励
回复