Weston 9.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Weston 9.0

Jump to solution
825 Views
sprado77
Contributor I

Currently, NXP BSP for iMX processors (L5.4.3_2.X.X) is based on Weston 8.0.

There are some new features in Weston 9.0 that could be useful in embedded applications, for example the kiosk shell (https://www.phoronix.com/scan.php?page=news_item&px=Wayland-Weston-Kiosk-Shell).

Also, Debian Bullseye and Yocto Project (Gatesgarth) already moved to Weston 9.0.

Is there any plan to move the BSP to Weston 9.0?

0 Kudos
1 Solution
816 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello sprado77,

 

Yes, we have plan to move weston 9 in next release, kernel L5.4.47 yet with weston 8. So one must wait for next release, in schedule to be ready early next year.

 

Regards

 

View solution in original post

1 Reply
817 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello sprado77,

 

Yes, we have plan to move weston 9 in next release, kernel L5.4.47 yet with weston 8. So one must wait for next release, in schedule to be ready early next year.

 

Regards