Webcam stream fails on ubuntu Notrogen6X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Webcam stream fails on ubuntu Notrogen6X

976 次查看
maitreyisharma
Contributor I

I have downloaded 20160802-nitrogen-4.1.15_1.2.0_ga-xenial-en_US-mate_armhf.img for Nitrogen 6X board

While booting I get follwoing error

 ov5640_read_reg:write reg error:reg=300a
adv7180 2-0020: adv7180_read:read reg error: reg=11 ret=-5
ili210x_i2c 2-0041: i2c transfer failed
ili210x_i2c 2-0041: Failed to get firmware version, err: -5
tsc2004_reset: write_cmd -5
tsc2004 2-0048: Failed to reset TSC -5
update_device_addr: ov5642 ret=-5
ov5642_read_reg:write reg error:reg=300a
update_device_addr: ov5640_mipi ret=-5
ov5640_read_reg(mipi):reg=300a ret=-5
mxc_v4l_open: Mxc Camera no sensor ipu0/csi0
mxc_v4l_open: Mxc Camera no sensor ipu1/csi1
mxc_v4l_open: Mxc Camera no sensor ipu1/csi0

On running the python program to capture video from Logitech Webcam it gives following error

uvcvideo: Failed to query (GET_CUR) UV.
uvcvideo: Failed to query (GET_CUR) UVC control 13 on unit 1: -110 (exp. 8).
uvcvideo: Failed to query (GET_CUR) UVC control 13 on unit 1: -110 (exp. 8).

What is the issue about?

I also tried to test the VLC player, that also gave me some problem.

0 项奖励
回复
0 回复数