WebGL and GPU acceleration issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WebGL and GPU acceleration issue

1,742 Views
sjpark
Contributor I

Hello.

I use wandboard(NXP i.MX6 Quad, ubuntu 16.04, vivante GC2000).
When I try "glxgears -info" and "glmark2-es2", it works fine with OpenGL ES 3.0.

But when I run the samples of "www.webglsamples.org" in the web browser, it doesn't work.
It seems that it doesn't support webgl although I set the browser's configuration correctly about "use hardware acceleration", "ignore software rendering list" and so on.

When I try the same thing in Yocto OS, it works fine.

What can I do for using webgl and hw accel  in this board and ubuntu 16.04?
Thanks in advance.

0 Kudos
Reply
1 Reply

1,662 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sean

webgl support is described in sect.5.1.4 Software Operation attached

Linux Manual and can be tested with Demo Images on link

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply