We found out the answer
Thank You igorpadykov and freescale team
Q1. We are not sure when the voltage change will reflect according to the new programmed voltages.
What the software flow for the changed voltages to reflect at PMIC output?
A1. a) For switching regulators, once a new target voltage value is programmed to correspnding register through I2C, the corresponding switching regulator output starts to transition to a new target voltage in voltage and time steps, shown in the Tables 34 and 35 of the MMPF0100 Data Sheet Rev.9 document, available on the Freescale web site:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMPF0100&nodeId=0143597440F744&fpsp=1...
b) For linear regulators, typical transition time is 1us to 10us depending on target voltage selected and actual load current. It also starts transitioning once being programmed.
Q2. In case of non programmed device , when we connect VDD OTP pin to ground we assume that MMPF will not give any output voltage even if PWR ON is asserted.
A2. Yes, you are correct.
Q3. also we would like to know the software flow for I2C programming in this case.
A3. There are two possible flows.
a) You can use the flow, described above. In that case, each regulator will start transitioning to its target voltage, once being programmed.
b) You can de-assert the PWRON signal, then program the complete configuration to MMPF, including desired power-up sequence, then assert the PWRON signal. The output voltages will start transitioning to programmed target values according to programmed power-on sequence, as described in the Section 6.1 "Start-up" of the document, mentioned above.