We are using i.MX6 Processor in our design. Is it required to provide POR reset signal for Processor Core Voltage, or the POR for processor core will be taken care by internal to the processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

We are using i.MX6 Processor in our design. Is it required to provide POR reset signal for Processor Core Voltage, or the POR for processor core will be taken care by internal to the processor

1,009 次查看
muralikrishna
Contributor I

We are using i.MX6 Quad Processor in our design. Is it required to provide POR reset signal for Processor Core Voltage, or the POR for processor core will be taken care by internal to the processor.

Kindly conform

标签 (1)
0 项奖励
回复
1 回复

848 次查看
Yuri
NXP Employee
NXP Employee

According to power up sequence of i.MX6 D/Q external POR signal is not mandatory :

"If the external SRC_POR_B signal is used to control the processor POR, then SRC_POR_B must

be immediately asserted at power-up and remain asserted until the VDD_ARM_CAP,

VDD_SOC_CAP, and VDD_PU_CAP supplies are stable. [...] In the absence of an external reset

feeding the SRC_POR_B input, the internal POR module takes control".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复