We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

Jump to solution
1,453 Views
geoffrodger
Contributor I

We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

0 Kudos
Reply
1 Solution
1,321 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello,

The official release date hasn’t published yet. If you want additional details regarding this topic, it is recommended submitting a Service Request ( www.freescale.com/support --> “Create Service Request”).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,321 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

On the following page you could find the Product Longevity chart, which includes life cycle of each family, and the lunched date, you could use it as reference:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=PRDCT_LONGEVITY_HM

Additionally, the part details page of MCIMX6X4AVM08AB indicates that it is Auto qualified, which means that its life cycle is more than 10 years; please refer to the following page:

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MCIMX6X4AVM08AB


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,321 Views
geoffrodger
Contributor I

Thanks Carlos.

Unfortunately the chart lists the i.MX6 SOLO but does not give the launch date.

I have found launch dates given as 2011 0r 2012 on the web. The rev0 datasheets are feb 2015.

Does anyone know the official launch date?

Regards

Geoff

0 Kudos
Reply
1,322 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello,

The official release date hasn’t published yet. If you want additional details regarding this topic, it is recommended submitting a Service Request ( www.freescale.com/support --> “Create Service Request”).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply