We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

跳至解决方案
1,499 次查看
geoffrodger
Contributor I

We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

0 项奖励
回复
1 解答
1,367 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello,

The official release date hasn’t published yet. If you want additional details regarding this topic, it is recommended submitting a Service Request ( www.freescale.com/support --> “Create Service Request”).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,367 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

On the following page you could find the Product Longevity chart, which includes life cycle of each family, and the lunched date, you could use it as reference:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=PRDCT_LONGEVITY_HM

Additionally, the part details page of MCIMX6X4AVM08AB indicates that it is Auto qualified, which means that its life cycle is more than 10 years; please refer to the following page:

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MCIMX6X4AVM08AB


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,367 次查看
geoffrodger
Contributor I

Thanks Carlos.

Unfortunately the chart lists the i.MX6 SOLO but does not give the launch date.

I have found launch dates given as 2011 0r 2012 on the web. The rev0 datasheets are feb 2015.

Does anyone know the official launch date?

Regards

Geoff

0 项奖励
回复
1,368 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello,

The official release date hasn’t published yet. If you want additional details regarding this topic, it is recommended submitting a Service Request ( www.freescale.com/support --> “Create Service Request”).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复