We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

ソリューションへジャンプ
1,464件の閲覧回数
geoffrodger
Contributor I

We are thinking of using the the MCIMX6X4AVM08AB in a project. Are there any estimates of how long it will be in production before it is replaced?

0 件の賞賛
返信
1 解決策
1,332件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello,

The official release date hasn’t published yet. If you want additional details regarding this topic, it is recommended submitting a Service Request ( www.freescale.com/support --> “Create Service Request”).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,332件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

On the following page you could find the Product Longevity chart, which includes life cycle of each family, and the lunched date, you could use it as reference:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=PRDCT_LONGEVITY_HM

Additionally, the part details page of MCIMX6X4AVM08AB indicates that it is Auto qualified, which means that its life cycle is more than 10 years; please refer to the following page:

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MCIMX6X4AVM08AB


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,332件の閲覧回数
geoffrodger
Contributor I

Thanks Carlos.

Unfortunately the chart lists the i.MX6 SOLO but does not give the launch date.

I have found launch dates given as 2011 0r 2012 on the web. The rev0 datasheets are feb 2015.

Does anyone know the official launch date?

Regards

Geoff

0 件の賞賛
返信
1,333件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello,

The official release date hasn’t published yet. If you want additional details regarding this topic, it is recommended submitting a Service Request ( www.freescale.com/support --> “Create Service Request”).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信