We are designing a custom Board based on MCIMX6Y2DVM05AA with eMMC boot. What are all the precautions to be taken for making the booting process smooth?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We are designing a custom Board based on MCIMX6Y2DVM05AA with eMMC boot. What are all the precautions to be taken for making the booting process smooth?

1,179 Views
theevanvenugopa
Contributor II

i.MX6ULL eMMC BOOT. 

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,045 Views
igorpadykov
NXP Employee
NXP Employee

Hi Theevan

first please follow Hardware Development Guide for the i.MX 6UltraLite Applications Processor
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf

Run ddr test

i.MX6/7 DDR Stress Test Tool V2.80 

Check power up sequence described in datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULLCEC.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply