Wayland GPU memory leak when opening and closing windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wayland GPU memory leak when opening and closing windows

1,852件の閲覧回数
stephenminutill
Contributor II

We are seeing GPU memory being leaked (seen with gmem_info) when a Wayland client process opens and closes multiple windows.  We are running kernel 3.10.53 and GPU software 5.0.11.p4.4 on an i.MX6Q processor.  How can we resolve this problem?  I see the release notes for BSPs which include 5.0.11.p4.5 seem to indicate this problem is fixed there ("MGS-528 [#ccc] Wayland does not free window memory until the application exits").  Can we use 5.0.11.p4.5 with a 3.10.53 kernel to fix the memory leak, while maintaining stability?  And will there be a patch release of a 3.10.53 based BSP which includes updated GPU software?

ラベル(2)
0 件の賞賛
返信
1 返信

1,317件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Stephen,

There are no available information about plans to release a patch for L3.10.53. So, the general recommendation could be using L3.14.28 to apply the currently available patch.

Unfortunately, not additional tests of the patch over L3.10.53 are available, so you could try, but considering the update changes from L3.10.53 to L3.14.28.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信