Way to update calibration values to DCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Way to update calibration values to DCD

Jump to solution
1,165 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about the way to update calibration values to DCD.

My customer is using i.MX6SL and making a boot image for SD boot.

They don't follow a way that is introduced following page.

https://community.freescale.com/docs/DOC-100203

They are directly updating bin file in the SD card using free tool such as Disc Editor.

I think I need to rebuilt a boot image every time.

Is there a possibility that the customer's way lead any problem such as boot fail ?

Ko-hey

Labels (3)
Tags (2)
0 Kudos
Reply
1 Solution
980 Views
Yuri
NXP Employee
NXP Employee

Hello,

   generally it is possible to edit the DCD values in binary form on SD directly.

Another way, that it is easier to introduce errors in such (manual) way.
And You should support some kind of log of modifications (again manually). 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
981 Views
Yuri
NXP Employee
NXP Employee

Hello,

   generally it is possible to edit the DCD values in binary form on SD directly.

Another way, that it is easier to introduce errors in such (manual) way.
And You should support some kind of log of modifications (again manually). 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply