Way to update calibration values to DCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Way to update calibration values to DCD

跳至解决方案
1,339 次查看
ko-hey
Senior Contributor II

Hi all

Let me confirm about the way to update calibration values to DCD.

My customer is using i.MX6SL and making a boot image for SD boot.

They don't follow a way that is introduced following page.

https://community.freescale.com/docs/DOC-100203

They are directly updating bin file in the SD card using free tool such as Disc Editor.

I think I need to rebuilt a boot image every time.

Is there a possibility that the customer's way lead any problem such as boot fail ?

Ko-hey

标签 (3)
标记 (2)
0 项奖励
回复
1 解答
1,154 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   generally it is possible to edit the DCD values in binary form on SD directly.

Another way, that it is easier to introduce errors in such (manual) way.
And You should support some kind of log of modifications (again manually). 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,155 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   generally it is possible to edit the DCD values in binary form on SD directly.

Another way, that it is easier to introduce errors in such (manual) way.
And You should support some kind of log of modifications (again manually). 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复